Are UART and USB both available for control of Boson, or is it either - or?

UART and USB virtual serial interfaces are both available for Boson camera configuration, however it is best to use just one.

The Boson USB-C adapter connects to the USB interface of the Boson. The Camera Link board uses an FTDI chip to connect to the Boson UART.  Either port can be used.