Knowledge Base
144 Results
FAQ
Can auto-exposure be turned on and off in Boson? Is auto-exposure used to normalize the image with respect to min and max pixel magnitude?
Read the StoryFAQ
Can FLIR provide the SDK documentation, or a list of functions controlled by the SDK, so we can make a decision on whether to order it?
Read the StoryFAQ
Can FLIR supply a thermal sensor without an IR window? Or, with a custom window? If not, how difficult is it to remove the window?
Read the StoryFAQ
Can lenses be interchanged on FLIR cameras? Will FLIR calibrate my lens with a Tau2 or Quark2?
Read the StoryFAQ
Can researchers with foreign nationality use a Boson, Tau2, or Quark2 camera at our facility in the U.S.?
Read the StoryFAQ
Can the FLIR start-up splash screen be disabled in Tau2 and Quark2 cameras? Can a different splash screen be used?
Read the StoryFAQ
Can the USB port on the Tau2 or Quark2 VPC accessory be used to just supply power, and use the coax connection for analog image?
Read the StoryFAQ
Can the video format of Tau2, Quark2, and legacy Photon cameras be changed from NTSC to PAL (or PAL to NTSC)?
Read the StoryFAQ
Do Boson, Tau2, or Quark2 meet any military environmental specifications or requirements?
Read the StoryFAQ
Do Tau2 or Quark2 cameras allow for thermography and temperature characterization?
Read the StoryFAQ
Does FLIR have any field failure rate data for Tau2, Quark2 that could be provided?
Read the StoryFAQ
Does FLIR offer or recommend software to run the gimbals, and what protocol does it use?
Read the StoryFAQ
Does operating Tau2, or Quark2, or legacy Photon cameras at less than 9 Hz reduce the camera power consumption?
Read the Story